Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge to SketchUp

Pioneer
Pioneer

I have a number of clients that require SketchUp's .skp files, until ST8 I used to use Sim Lab's add-in to convert my .par and .asm files - that add-in no longer works.

 

Is anyone converting Solid Edge .par and .asm files to SketchUp file .skp format? If so, what are you using, or how do you do it without some type of converter add-in?

 

- Thanks

 

I should have noted the import file formats that SketchUp will accept when I first posted, they are:

 

.dwg

.dxf

.3ds

.dae

2 REPLIES

Betreff: Solid Edge to SketchUp

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

whats about the new ifc files in ST8?

Will the work?

 

 

regards

Wolfgang 



regards
Wolfgang

Betreff: Solid Edge to SketchUp

Pioneer
Pioneer

No, unfortunately it won't.

 

SketchUp is very limited on what it will accept; SE will, of course, export a number of formats, just not the ones that SketchUp will accept. I have been in touch with Sim Lab, the company that makes the addin that I have been using in the past, I seem to get different answers everytime I ask about them updating to work with ST8 - one day it's no the next week it's yes.

 

Thanks for the suggestion.

 

Dave