Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge with Agile PLM

Experimenter
Experimenter

Hi

 

Can anyone plese guide me how to configure the SolidEdge with Agile PLM.

 

3 REPLIES 3

Re: Solid Edge with Agile PLM

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What do you need help with?  There is nothing in Solid Edge that needs configured to work with Agile PLM.  You just need to install the EC Connector for Solid Edge from Xplm and then there is some configuration with Agile PLM and the EC Client.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge with Agile PLM

Experimenter
Experimenter
Hi ,

I am not getting any link to download MCAD connector. Can you please help
me with steps to configure solid edge with Agile PLM.

Thanks & Regards
Anand

Re: Solid Edge with Agile PLM

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@RapidPLM, the Agile EC Connector for Solid Edge is available from Oracle's Software Delivery Cloud given you have an account under which you purchased a license for the software.  If you do not have such an account, you can contact Oracle Agile PLM sales to purchase a license.  Since you have Agile PLM, I'm guessing you are already familiar with your Oracle Account Manager.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com