Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge with Teamcenter and replace a part with copy

Experimenter
Experimenter

Hi Edgers!

 

I use Solid Edge with Teamcenter and when I want to Replace a part with copy this problem appears.

It only appears with one assy.

problema2.png

 
Does anyone know what happens?
 
 
Thanks,
 
8 REPLIES 8

Re: Solid Edge with Teamcenter and replace a part with copy

Gears Phenom Gears Phenom
Gears Phenom

A bit more detail and a screenshot of the entire monitor would be helpful.   But seeing your other post as well...  Seems like something is acting up with your CPD...  have you closed SE and REbooted your PC?

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Solid Edge with Teamcenter and replace a part with copy

Experimenter
Experimenter
Yes,

I reboot the SE and the PC and that is still happening.

whats CPD?

Re: Solid Edge with Teamcenter and replace a part with copy

Gears Phenom Gears Phenom
Gears Phenom

CPD = Common Properties Dialog   - the window that pops up to see the files props and perform the save action,

 

Can you have another user log in to this same PC and retest?   This will test the SE HKey Current User Reg Setting.  IF another user can log into Windows on this PC and then log into SEEC and perform the same actions without issue we can rebuild the REG

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Solid Edge with Teamcenter and replace a part with copy

Experimenter
Experimenter
This issue appears in all users. But the other one only in one user.

Re: Solid Edge with Teamcenter and replace a part with copy

Gears Phenom Gears Phenom
Gears Phenom

@xe    Is this a new issue?  Has it worked correctly previously? 

Have you tried to use cache asst to manually clear the cache?

I wonder if something is trying to process and that pops up the CPD during the Replace command?

 

might try to close, checkin in, clear cache, delete cache folder, delete SEEC Trans Log.  Reboot and Retest?

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Solid Edge with Teamcenter and replace a part with copy

Experimenter
Experimenter
Yes its new.

We have found a solution, doing the save as with the structure manager

Re: Solid Edge with Teamcenter and replace a part with copy

Gears Phenom Gears Phenom
Gears Phenom

I would not consider this resolved,  you will need the SEEC UI to work correctly.

 

Since this is a new set up and is not working correctly I'd get with your Install team and get this resolved.

 

Something is not right.   - obviously...

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Solid Edge with Teamcenter and replace a part with copy

Pioneer
Pioneer
It looks to me like your missing columns, or one is stretched out to large. Try playing with the columns to be sure you are not missing any.