Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Solid edge Queries

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello All,

 

1. In sheet metal can we do rolling of a sheet to a cylindrical shape without it be been created as a cylindrical sketch.?

2. Do we have any option to measure the weld length after doing the welding ..?

3. Once we do a circular drawn-cutout can we take a flange from that particular drawn-cutout..?

4. Can we add SEAM Welding also to the welding options?

3 REPLIES 3

Re: Solid edge Queries

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

4 questions and a solution video:

 

 

1. Yes, I suggest using Feature Library...

2. Yes, you should be using Measure command and save length

3. Yes, but not directly

4. Yes, If I understand correctly

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Solid edge Queries

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you very much. Smiley Happy

Can we bend the flat sheet metal into cylindrical shape??

Re: Solid edge Queries

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, this depends on your challenge! Smiley Wink

 

 

BR,

Imics
http://solidedgest.wordpress.com/