Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid edge ST6 - install standard parts

Experimenter
Experimenter

Hello,

I have problem with installing standard parts to my ST6.
Run (as a admin, i have win 7) standard parts configuration wizard to set locations of parts --> tried all location options, but with no success (see below).

There is some database error with no specify. Also i have tried reinstal SQL server express from Microsoft.

Any ideas where is the problem?

Thank you in advance

 

 

 

error.JPG

3 REPLIES 3

Re: Solid edge ST6 - install standard parts

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

have seen this before and all indications are that you have a bad sql install.

 

I suggest doing a complete removal of sql including all regestries!  

 

also uninstall std parts and then reboot

 

Then try to reinstall std parts.

 

Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/

Re: Solid edge ST6 - install standard parts

Builder
Builder

Also check in SQL Server Services that SQEXPRESS is running. It should be Running, and set to start Automacally.

Re: Solid edge ST6 - install standard parts

Experimenter
Experimenter

Guy ,

 

try to run the wizard as admin . Moreover , check if you have write permission to the selected server path .

 

Dudi