Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid edge ST9 too slow

Experimenter
Experimenter

My ST9 It is also slow with very simple files.

PC= Fujtsu celsius W550W3

intel Xeon E3-1275v5 3.6GHz 16GB ram DDR-4 2133MHz 

Solid State Hard Drive

Nvidia QuadroM2000 16Gb driver 385.901

Windovs 10 pro 

Monitor EIZO 32" EV3237

All updated with the latest releases.

what can I do?

 

7 REPLIES 7

Betreff: Solid edge ST9 too slow

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Sandro-2

 

 

 

sorry to hear that, but I think You should further explain, what is slow?

 

Your hardware specification sounds well, I have an much older and not so good workstation here, doing a good job.

So Your system should perform even better, without any problems or slow downs.

 

But again, what is slow?

 

 

regards
Wolfgang

Betreff: Solid edge ST9 too slow

Experimenter
Experimenter

for example.

I'm in iso part.
I create a solid one.
I create a hole.
turning in to hole options, the window opens slowly.
the icons appear one after the other slowly.
it takes about 4 seconds.
I work in an ordered option.
 

Re: Solid edge ST9 too slow

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Head to Options (Application button > Settings > Options) in a new part environment, and in the view tab > application display, choose graphics card driven (advanced) or just graphics card driven.

This has fixed up the issue for me so many times that I can't even recall.

Capture 1.JPG


Paras Raina, Technical Head, MSC Systems Pvt. Ltd. (India)
NX 12.0.2
Solid Edge 2019

Betreff: Solid edge ST9 too slow

Siemens Phenom Siemens Phenom
Siemens Phenom

What version of Windows 10 Pro are you using? If it is the Fall Creators Update (version 1709), you are likely seeing the issue being discussed in this thread:

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/ST9-Dialog-windows-slow-down/m-p/44...

 

The symptoms you describe sound the same.

 

Greg

Re: Solid edge ST9 too slow

Experimenter
Experimenter

thanks for your advice.
but the options were already set

Betreff: Solid edge ST9 too slow

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@GregLuckett  Any idea when MS may be addressing this in a Windows fix or a fix SPLM can provide?



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: Solid edge ST9 too slow

Siemens Phenom Siemens Phenom
Siemens Phenom

@KennyG I really don't know. RD is the one who has been working with them.

 

Greg