Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid edge St 10 material table crash

Experimenter
Experimenter

Hello

I got an issue, If I want to select a material in solid edge than solid edge crash.

Have sombody a solution for this problem?

 

1 REPLY 1

Betreff: Solid edge St 10 material table crash

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Beau

 

 

as usual here in the Academic Forum I have to ask the first standrad question:

 

ST10 with the MP3 or ST without any MP?

 

If no MP then I would suggest to download the later ST10 file with MP3 included, or, if You are at a UNiversity with maintenacne contract (Solid Edge University version) then ask Your prof to take care about the current MPs

 

On the other hand, I do not now about any issues when assigning a material to an open part.

So let mes ask following question too: Which material file are You using?

The standard MTL delivered with ST10 or maybe an old one from a former version?

 

 

regards
Wolfgang