Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Solid edge draft (free) won't start/load

Not applicable
Sometimes when starting solid edge draft ( latest release ) from the windows vista home premium program start list I get the first graphic screen of draft starting and then the windows message:

" Solid edge has stopped working" - A problem caused the program to stop working correctly windows will close the program and notify you if a solution is available.

After a couple of attempts the program with then load and I am able to use.

Please advise.

Thanks,

Jason Guest
1 REPLY

Re: Solid edge draft (free) won't start/load

Not applicable
I reinstalled the solid edge draft software after removing the old upgraded version and removed the hardware acceleration from my nvidia card and that seems to have solved the trouble for now.

Thanks,

Jason