Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid edge plane setting

Experimenter
Experimenter

Hi guys. hi have a problem when i want to set a plane to see a secxtion view.

see image attached. Is this a setting that can be fixed?

4 REPLIES

Re: Solid edge plane setting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not sure what the problem is for you.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Solid edge plane setting

Siemens Phenom Siemens Phenom
Siemens Phenom

What is the exact issue?  Setting the location of the plane?  Plane transparency?

Kevin Grayson
Solid Edge Technical Consultant
kevin.grayson@siemens.com

Re: Solid edge plane setting

Experimenter
Experimenter

yes plane transparency

Re: Solid edge plane setting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For the Dynamic Clipping planes, the settings are in the Solid Edge Options on the View form towards the bottom.  You can select a color for each plane and a transparency.  Be aware that if you make the planes transparent, you will not see a solid sectioned model colored face of cut models but instead they will appear hollow.  If you want a true section view with solid section faces of the model color, use the Section command in the Model Views section of the PMI Ribbon tab.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com