Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid edge running on an APU?

Builder
Builder

Has anyone used solid edge on any apu? Does it work well?

2 REPLIES

Re: Solid edge running on an APU?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The Surface Pro 3 uses an APU and Solid Edge works rather well on it.  In fact many folks have tried out the Intel APU's with Solid Edge and as long as you are using an HD graphics version that supports the Solid Edge graphics requirements they work quite well.  Not sure about AMD's APU offering.  Their Radeon integrated graphics have never been that good with SE and I'm not sure if they even have workstation class APU's with FirePro graphics.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Solid edge running on an APU?

Builder
Builder

Thanks. I do know there are pro versions of their latest flagship APU Kaveri. How good they work I would like to know.