Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid edge st6 on a 32bit win7 machine error opening sev file

Experimenter
Experimenter

Im attempting to open the goblin v2 sev file from the greenpower site on the st6 student edition on a windows 7 32 bit machine but get an error message which says :

 

"no translator is available for this file type"

 

any ideas please?

 

Im a complete novice on this but need to access side, top and front views of the v2 goblin for the kids at school.

 

Many thanks

 

2 REPLIES 2

Re: Solid edge st6 on a 32bit win7 machine error opening sev file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Can't say for sure, but guessing the files were saved in a more recent version of Solid Edge since ST6 is about 4 years old now.  The files are not backwards compatible with older versions of the software once saved in a newer version.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid edge st6 on a 32bit win7 machine error opening sev file

Experimenter
Experimenter

Thanks.

 

Looks like Ill have to upgrade the computer to be able to do anything then.

 

Would you be able to do me a massive favour and take screenshots of the car for front, side and top views and send them to me if I let you have the file and a contact email?

 

Thanks

 

Allan