Cancel
Showing results for 
Search instead for 
Did you mean: 

SolidEdge ST9 has stopped working

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi all,
Previously it was ST8 now upgraded to ST9. After installation finish, I have started SolidEdge, it's loading and solid edge stopped working tab poped-up. I have double check the installation process and found that femapapi.exe "the application couldn't start correctly (0xc0000001d).

Is anyone have the same issue here?

Thanks
Destian
3 REPLIES

Re: SolidEdge ST9 has stopped working

Honored Contributor
Honored Contributor

0xC0........... 

Typically a vid card issue. Try upgrading vid card drivers to current.

Re: SolidEdge ST9 has stopped working

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi 12GAGE,

Thanks for the reply, i have checked in windows log event viewer the problem was "windows update failure". I have noticed them to update the windows. I'm not sure yet whether the issue will be solve. I need to check again after they update the windows.

Re: SolidEdge ST9 has stopped working

Honored Contributor
Honored Contributor

I have needed to reboot SE (or the entire computer) just because windows was downloading an update. The random problems would continue until I let windows perform the update.

 

Good luck.