Cancel
Showing results for 
Search instead for 
Did you mean: 

SolidEdge Viewer permissions

Not applicable
I cannot open any files in Solid Edge Viewer unless I have Administrator privileges on my machine. Otherwise, I get "Failed to Open Document".

Is there a workaround? Right now, the user has to open the file with Solid Edge 2D instead.

Regards
6 REPLIES 6

Re: SolidEdge Viewer permissions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Which version are you using? One of the versions had a delivered bug where Viewer had to be run with Admin rights to works which was fixed with a subsequent patch to the full product.


Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: SolidEdge Viewer permissions

Not applicable
Hi Ken -
I'm using Solid Edge 2D Free ST5.
I tried downloading and installing Solid Edge Viewer ST6 but when I attempt to install it, it warns me that I cannot because another version is installed. I can't uninstalled Viewer ST5 without also removing 2D Free ST5.
Regards

Re: SolidEdge Viewer permissions

Not applicable
Ken or Rick - any resolution to this?

Re: SolidEdge Viewer permissions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
SE installs a version of the viewer so you cannot install the standalone viewer in addition. You would have to uninstall SE completely to test the ST6 viewer or install SE ST6 Free 2D when available.


Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: SolidEdge Viewer permissions

Not applicable
So if I uninstall ST5 Free, install Viewer 6, and then try to re-install ST5 Free....will it leave the ST6 viewer alone?

Re: SolidEdge Viewer permissions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
No, you will not be able to install ST5 if the ST6 Viewer is installed. You cannot have the Viewer and SE installed at the same time, even if they are different versions.


Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com