Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Solidedge 2019 Now Embossing Email Address in Draft Prints

Pioneer
Pioneer

Hi,

 

I downloaded Solidedge 2019.  Now when I try and print one of my drafts, an email address gets embossed at the bottom of the page.  I'd like for that not to happen but I see no option to change it.embossed.JPG

 

I am using a solid edge startup license that's good for one year.  Not sure if this is causing the problem?

4 REPLIES 4

Re: Solidedge 2019 Now Embossing Email Address in Draft Prints

Gears Phenom Gears Phenom
Gears Phenom

Are you sure that is not in your PDF settings?  I am not aware of any SE function that would put that there.

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Solidedge 2019 Now Embossing Email Address in Draft Prints

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Johnson_BigMatt 

 

 

I know that certain SE versions (licenses) like academic and demo will put a watermark to that position.

So it also might be possible, that  startup licenses will leave a watermark too.

 

 

regards
Wolfgang

Re: Solidedge 2019 Now Embossing Email Address in Draft Prints

Siemens Phenom Siemens Phenom
Siemens Phenom

Startup licenses are full blown Solid Edge licenses without any restrictions.  This also includes no watermarking.

 

Therefore any watermarking is *not* because of the startup license.

 

I would hazard a guess that because the user is printing to Adobe PDF as the printer that this is a function of the settings within the Adobe PDF printer.

Re: Solidedge 2019 Now Embossing Email Address in Draft Prints

Pioneer
Pioneer

I had to reinstall Solid Edge but was never prompted for a license file.  It looks like I may have been on a trial license.