Cancel
Showing results for 
Search instead for 
Did you mean: 

SolidedgeTranslationService.exe (Select multiple files)

Pioneer
Pioneer

Hello.
With title
Solidedgetranslationservice exe file of several using the file dft dwg to change to the file.

 

ex>

SolidedgeTranslationservice.exe -i=c:\test\*.DFT -o=c:\test\*.DWG -t=dwg  <--Is that possible?

 

I'd like to make a batch file using cmd..

 

And you need a way to add to mouse right button.

 

Thankyou

3 REPLIES

Re: SolidedgeTranslationService.exe (Select multiple files)

Siemens Phenom Siemens Phenom
Siemens Phenom

You can only pass one file at a time to the SolidedgeTranslationService.exe command line.


Check out my blog post on using SolidEdgeTranslationServices.exe:

 

http://community.plm.automation.siemens.com/t5/Solid-Edge-Blog/Translating-Solid-Edge-Files-from-the...

 

The last graphic in that post shows what you are asking -- creating a mouse button right-click: 

10.png


So yes, it is more than possible to do what you want with some simple DOS or PowerShell scripting and registry hacks.

Re: SolidedgeTranslationService.exe (Select multiple files)

Siemens Phenom Siemens Phenom
Siemens Phenom

P.S.  If you check out my GitHub site you will find an unfinished [but working] project that does exactly what you are asking for, including adding the Windows Explorer registry entries of the right-click menu:

 

https://github.com/uk-dave/SolidEdge/tree/master/SolidEdgeTranslateFromExplorer

 

 

Re: SolidedgeTranslationService.exe (Select multiple files)

Pioneer
Pioneer

Thank you~ Dave..