Cancel
Showing results for 
Search instead for 
Did you mean: 

Solidworks data migrartion

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi

 

Has anyone run the sw data migration?

 

At first look it seems that you can only do one folder at a time? This seems to be a big limitation to me as people will quite often have files spread through multiple folders and to have to do this one folder at a time would be very tedious.

 

Is there a way top pick a top level folder and get it to do all sub-folders?

2 REPLIES 2

Re: Solidworks data migrartion

Siemens Phenom Siemens Phenom
Siemens Phenom

At this time the SolidWorks migration can only select one folder and it will not process sub-folders.


As a Partner, I would suggest that you cant GTAC and submit an IR for this.

Re: Solidworks data migrartion

Phenom
Phenom

Ouch...In my opinion, that's a serious issue.

As a SW admin, I've seen folder structures that were 10-15 levels deep for a project or the almost infinite amout of folders inside the SW EPDM archive server (where all files are saved within EPDM).