Cancel
Showing results for 
Search instead for 
Did you mean: 

Split a Symmetric Offset

Not applicable

If I use the Symmetric Offset to create a detail, can I split the created element
into lines and arc with endpoints?
2 REPLIES

Re: Split a Symmetric Offset

Not applicable
Currently, the answer is no. The geometry created from the symmetric offset
command is a single unit.

Re: Split a Symmetric Offset

Not applicable
You can however perform an "include" or "tear off sketch" of the symmetric
offset into another sketch which will yield lines and arcs.
--
Ken
http://grundey.blogspot.com
"Ricky Black" wrote in message
news:465c33e3$1@bbsnotes.ugs.com...
> Currently, the answer is no. The geometry created from the symmetric
> offset command is a single unit.
>