Cancel
Showing results for 
Search instead for 
Did you mean: 

Standard Part Library Installation

Phenom
Phenom

I use "Systems Parts 4" for years now to insert nuts & bolts.

I tried again to install standard part library, but can't do it...

I don't understand what's wrong, nor what I have to do.

After installing the administration from DVD1 and the parts from DVD2 I try to enter the configuration wizard but receive:

Standard.png

What now??

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user
10 REPLIES 10

Re: Standard Part Library Installation

Genius
Genius

Hi Joris,

 

Have you tried to fill in a UNC path for the top level folder? Something like:

 

\\PCname\Solid Edge Standard Parts

Re: Standard Part Library Installation

Phenom
Phenom

Thanks, but this is not the solution:

name.png

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: Standard Part Library Installation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Joris,

 

I have seen this error when Standard Parts waws installed with UAC on...

 

IJsbrand

Re: Standard Part Library Installation

Genius
Genius

Hi Joris,

 

Try again and make sure ALL paths are in UNC notation (click the Defaults button).

 

Configuration Wizard settings 1.JPG

Re: Standard Part Library Installation

Phenom
Phenom

I changed it all but the same error...

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: Standard Part Library Installation

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Have you defined the working database?  Have you read the Standard Parts Installation Guide?  It is a file called StandardPartsInstallationGuide.pdf and it is located at C:\Program Files\Solid Edge ST6\Program\ResDLLs\0009.

 

Are there multiple users using Standard Parts or are you a one-man band?  If there are multiple users then UNC paths must be used in the configuration wizard.  Otherwise their SE installations will think the Standard Parts database is in their C-drives...

Re: Standard Part Library Installation

Phenom
Phenom

Can someone please explain me why it is such a PITA to install a program???

 

I use for years Systems Parts from Stream Design, the installation is: "Install"

When you want to use it over a network you just point to the place and that's it.

 

Now for SE:

Dig in the catacombs of the program folder and search for pdf file.

Yes I found this file, no it doesn't help

 

Both programs are from the same company. TALK TO EACH OTHER to streamline this.

It can't be possible this leaves the house with a stamp "approved".

The installation of SP should be a check box in the SE installation.

 

I am just trying to install on my PC for me only. One step at a time...

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: Standard Part Library Installation

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

look at your Microsoft.net Framework. i had to roll mine back to 1.1 to get it to work

Re: Standard Part Library Installation

The Standard Parts new interface with the SQL server is really bad. From ST6 to ST7 I had to import every single component, took me 2 days.
I was glad that our Dutch support could set the first system (believe ST1) this because otherwise we would still not running this system.
-------
Daniël Schuiling