Cancel
Showing results for 
Search instead for 
Did you mean: 

Standard Parts Administrator

Valued Contributor
Valued Contributor

I have a Startup copy of Solid Edge that I qualified for.  I am trying to install standard parts from the downloads section (where we can download MPs and such).  I see there is the Standard Parts install, but I do not see a Standard Parts Administator available to download.  How can I go about getting these standard parts library installed!?

33 REPLIES

Re: Standard Parts Administrator

Legend
Legend

This worked for me on ST9, I assume it is the same for ST10

 

Your are looking in the right place.

Download the appropriate Solid Edge DVD (eg.  Solid_Edge_DVD_ENGLISH_ST9.exe )

 

Once you have the DVD unpacked you can go to the DVD folder and run autostart.exe (there is no need to burn the DVD it will run from your hard drive).

 

From there you can run the Standard Parts Administraton

Solid Edge 2019 MP4 - Windows 10 - K2000

Re: Standard Parts Administrator

Valued Contributor
Valued Contributor

Thank you for that.  I did find it and install it but still cannot get it to do right as I cant find the .sac file.  I have never in my life sen something so hard to install.....

Re: Standard Parts Administrator

Legend
Legend

I can't remember how I installed it, but there should be a pdf with instructions for how to install it. It is in the DVD you downloaded.

 eg. Solid_Edge_DVD_ENGLISH_ST9\DVD\Standard Parts Administration\StandardPartsInstallationGuide.pdf

 

There is also a detailed guide here:

https://community.plm.automation.siemens.com/t5/Solid-Edge-Blog/Standard-Parts-Installation-of-Stand...

Solid Edge 2019 MP4 - Windows 10 - K2000

Re: Standard Parts Administrator

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @lifofadrafter

 

 

 

the first You must do is to install the "Standard Parts Administrator" from the Solid Edge base DVD (image) as described before.

 

Here a good tip will be, to install at least one of those example parts (DIN, ISO, ANSI, doesn't matter which, but at least one of this group).

This is necessary to install a correct SQL Express database on Your computer.

After doing that You should find a Configuration assistent (wizzard) under Your Solid Edge Programs Group.

 

Start it and - that's my setting - turn of a version number for standard parts - and save this config.

If You here will see and successfully save, then everything is OK.

If not, then there is no reason for continuing the installation.

Check and try as long as this will be successfully done.

 

Now You can install the machinery library from a different installation image (extra download).

Select those parts which are important to You and install them

 

And please don't think, that You have done it now.

No.

 

Now You must open the Standard Parts Administrator and add these new library to the database.

Or - and this is possible from ST9 upwards, You can select to add the library duringthe machinery libraryinstallation too.

This will lead to an database upgrade/update/installation (call it as You like) which will take at lest one hour, maybe longer depending on the disc speed of Your computer and the number of standards You have selected

 

Most things are described witihn the Standard Parts Installation Guide.

 

 

Finally I only can say:

 

"Good luck!"

Hope it works!

 

 

regards
Wolfgang

Re: Standard Parts Administrator

Experimenter
Experimenter

Hi Edgers,

 

I am trying to install Standard Parts but cannot find the Administrator EXE within the files from DVD.

I extracted SE Standard Parts.exe. 

 

Can anyone tell me where it is placed?

 

Thank you,

Regards,

Arek

Re: Standard Parts Administrator

Phenom
Phenom

Hi @hawcad

Hi Wolfgang,

 

I have got a question regarding SParts installation.

I have installed the Administrator but when I try to open this app nothing happens.

 

Have you spotted this before?

Thanks

Arek

 

Re: Standard Parts Administrator

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @leec7

 

 

the Standard Parts Admin installer is found in the basic SE Installation image not in the Standard Parts DVD

regards
Wolfgang

Re: Standard Parts Administrator

Phenom
Phenom

Hi @hawcad

 

Leec7 is my second account.

 

Yes, right, I found it finally.

the problem has explained a post above.

 

regards,

Arek

Re: Standard Parts Administrator

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @arekkul@leec7

 

have You installed the example databse when installing the Admin?

This is necessary to get the SQL database configured correctly.

 

And when You say, nothing happens, what are You trying to start/run?

 

 

 

regards
Wolfgang