Cancel
Showing results for 
Search instead for 
Did you mean: 

Standard Parts in Student Edition

Experimenter
Experimenter

Hallo,

 

habe folgendes Problem. Ich habe die Student Edition von ST8 runtergeladen. Meine Frage ist jetzt wie kann ich die Standard Parts installieren? Habe beim ausführen der .exe keine Möglichkeit die zu installierenden Module auszuwählen.

 

Kann mir da irgendjemand helfen?

 

Mit freundlichen Grüßen

Steven Schreck

1 REPLY

Re: Standard Parts in Student Edition

Community Manager Community Manager
Community Manager

@Duke194

Run setup.exe from Standard Parts Administration folder. Complete the installation.

This setup delivers some sample files from various standard (ANSI, DIN, ISO, GOST etc.)

 

You can find the Standard Parts installation document  on how to install the Standard Parts in “StandardPartsInstallationGuide.pdf” at "C:\Program Files\Solid Edge ST8\Program\ResDLLs\0009".

 

If your problem is not resolved with above suggestion then please let us know the exact problem with steps so as to give appropriate solution.