Cancel
Showing results for 
Search instead for 
Did you mean: 

Standard Parts

Experimenter
Experimenter

I have a problem tot add Standard Parts in the Administrator. I want to use the installed MachineryLibrary_EN_V15_00.ddb

I get an Error "Selected database is not valid. PLease select a correct one. When I try older versions I have te same error.

 

Can somebody help me? Thx a lot2018-08-05_23-25-43.png

6 REPLIES 6

Re: Standard Parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Filiep,

 

Maybe >this Blog post< can be of help.....?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: Standard Parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Filiep

 

 

 

I remember similar problems a time ago.

 

So if You are using ST9 or 10 then it could be, maybe, that the masterparts DB is corrupted and will not work for installation.

Try the installation with a given folder - parent parts - instead.

This helped for me.

 

regards
Wolfgang

Re: Standard Parts

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

In this case use following option:

"Add from existing multiple parts" and next, next, next... Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Standard Parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Imics

 

This is what I thought to be with my last post "... existing folder ..."

And I did not look onto the picture.

 

But thanks and Yes @Filiep, this should work for You at all.

 

BTW: which SE version are You using?

I hope that this issue is fixed for SE2019?

regards
Wolfgang

Re: Standard Parts

Experimenter
Experimenter

Thx a lot it works

Re: Standard Parts

Experimenter
Experimenter

I use Solid Edge ST10 MP9