Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Standard not open in solid edge

Creator
Creator

I have successfully installed the "Standard Part" but I cannot open it or choose Sac file in solid edge

It does not react. Screenshot (47).pngI can open it at windows.

Excuse my English

Screenshot (48).pngScreenshot (49).png

1 REPLY 1

Betreff: Standard not open in solid edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Evil 

 

 

the question is,  what have You installed and how have you done this.

 

Standard parts installation begins with the Standard Parts Admin, what also initialize the SQL database.

Then go to the configuration, check all entries and settings and confirm them.

This should be answered by the successfully install message box.

 

Now You can add the library and update the database.

 

Afterwards the standard parts should be ready for use.

 

Finally comes the question: "Do you have the license too?"

 

 

regards
Wolfgang