Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: Standard parts administer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad  Got it! I was pleased to see that if the new location where you use saved settings needs a longer screw that the software adjusts for it. Nice.

Thanks!

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: Standard parts administer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @bshand

 

 

this is what Fastener System always should do for You, do check how long the bolt must be to fit to the given situation.

 

IMHO there only is one issue or improvement, I would like to see within fastener, and that is the possibility to use it for blind holes too, and not only for through holes.

So that You will get the maximum length of a screw too, not only the minimum length.

But to be honest, this more or less is a cosmetic issue rather than a real technical problem.

 

 

 

 

regards
Wolfgang