Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Re: Standard parts and Insight

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

configwiz.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Standard parts and Insight

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Can you send a screenshot of the filelocation in Solid Edge Options?

 

Also for interest is your structure of the SharePoint. Which is the Site, the Doclib and the Folder

\\sql\RelSite\StdPrt\Genpart

 

We usually have configured that the Standardparts are directly saved in a Doclib. As far as I can see ist that you save in a folder. Never tried but I will test this!

 

Do you still have the origin configuration from Insight (WSS 2.0) with the different sites? (WIP Site, Rel Site, Ops Site, etc.). It can be a problem of cross site working? We have moved all customers to a single site configuration with doclibs so we have no experience with it.

 

Stefan

smitsch@unitec.de
www.all4edge.de

Re: Standard parts and Insight

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

As far as I know our 3 main sites: PreLib, RelLib and ObsLib are all document libraries.

 

filelocs.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200