Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Start Solid Edge in Background

Innovator
Innovator

Is it possible to start Solid Edge ST 8 in Background?

3 REPLIES 3

Re: Start Solid Edge in Background

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @Sonya

   

This is possible using the Solid Edge API which involves programming.

What is the purpose of starting SE in background; can you give more information ?

   

Tushar

 

Re: Start Solid Edge in Background

Innovator
Innovator

Hi @Tushar

 

we would like to check some cad data and we need to open evry data in solid edge in batch mode in order to save time
we will process many cad data.

thanks

Re: Start Solid Edge in Background

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Sonya

 

 

 

so this is not the problem.

 

 

If You take a look into the batch program (in custom folder of Solid Edge)  You will find the appropriate code for setting the SE start as non visible and without user interaction, which defaacto is background mode.

 

 

regards
Wolfgang