Cancel
Showing results for 
Search instead for 
Did you mean: 

Static Study Simulation of Assmely

Experimenter
Experimenter

Hello,

 

We are trying to do static simulation of assmebly.  Few questions.

 

1) The force is requried to be entered,  when in put the load (force) as 2000 kgs, the report show force force as 2e+003 mN.  Please explain this unit of Force (mN). 

 

2) We would like to have force diagram and contrainst diagram of the assembly in the report.

 

Please explain for the above.

 

thanks

 

 

3 REPLIES

Betreff: Static Study Simulation of Assmely

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @3D-DESIGN-DTPL

 

IMHO there is not much to explain.

 

The standard unit of force is [N] (Newton) and a subunit as for all other units might be [mN] (milliNewton)

 

[kg] is the unit of mass but not forces

 

Which default units You want to use can be defined in the option tab unit

 

 

regards
Wolfgang

Betreff: Static Study Simulation of Assmely

Experimenter
Experimenter

Thanks you for your explanation.

 

I think we would be able to resolve our issue with your reply.

 

we appreciate 

Betreff: Static Study Simulation of Assmely

Gears Phenom Gears Phenom
Gears Phenom

@3D-DESIGN-DTPL,  if @hawcad's helped solve your issue...  

 

For the sake of all in the community... Please consider giving KUDOS to answers that were helpful to you or appreciated. Also please mark a post as the SOLUTION if you feel you received an answer. This helps give credit and creditability to other users and helps others find a solution in the future when searching the forums.
thanks!


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7