Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Re: Steel shapes: Drafting or engineering dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@RyanM It kind of sounds like you are getting hung up on the nominal dimensions vs. the toleranced dimensions shown on the print.  Like others have said, you always model to the desired value (7 places...) but then you detail to the expected manufacturing tolerance.  If that is 1/16th of an inch, then that's what you round to.  I imagine your structural steel guys are measuring their cuts with a tape measure and accuracy less than 1/16th is a "pie in the sky" wish.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Steel shapes: Drafting or engineering dimensions

Phenom
Phenom

Ken you are correct. They are taking the hole punch out into the field (in some cases) and then putting in the holes based on measuring tape. Like I mentioned just wondering what people are actually doing for model geometry.

If you were to ask this question on a Autodesk forum I'm sure we would get a different answer. ;-)

Re: Steel shapes: Drafting or engineering dimensions

Honored Contributor
Honored Contributor

I actually display 3 digits unless the dimension comes out to a 1/16" fraction of some kind. Then I display fractions. The tape measures are in 1/16 or 1/32. However, most machines allow you to enter 3 digits. Like a punch, folder, etc....

 

So every dimension, you have to think about how and who is going to use it.