Cancel
Showing results for 
Search instead for 
Did you mean: 

Stitched Surfaces Do Not Create Solid in synchronous Surface Creation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi

 

I have a created a enclosed surfaces and when these surfaces are stiched togeather it is not converting to solid. 

 

I found a solution in http://www.eng-tips.com/viewthread.cfm?qid=318351 and the solution is

 

Take what you have done and re-apply the stitch command. Then select "stitch" from the feature tree, right click and select "attach", then select "add".  This will give you a solid.

 

But it is not working for me, I didnt find ADD after the attach operation.

 

Any help...

 

Rgds

 

Rajkumar | i-Value Tech Solutions

www.i-vtech.in

7 REPLIES 7

Re: Stitched Surfaces Do Not Create Solid in synchronous Surface Creation

Phenom
Phenom

From memory ,the 'add' command will only appear in synchronous mode so if you're in ordered you won't see it. Otherwise, are you 100% sure your surfaces are all stiched together with no holes?

 

Maybe upload your file so we can test? 

Re: Stitched Surfaces Do Not Create Solid in synchronous Surface Creation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi 

 

I am in Synchronous Mode Only. Please find attached the file for your reference.

 

Rajkumar

www.i-vtech.in

Re: Stitched Surfaces Do Not Create Solid in synchronous Surface Creation

Phenom
Phenom

@Raj_I-value, I'm on ST7 so can't try it for you, but maybe someone else will.

 

However, instead of seeing 'Add or Substract', are you getting a red arrow on screen asking you to select the direction to attach? If so, I think your sticked surfaces aren't fully enclosed.

 

Alex

Highlighted

Re: Stitched Surfaces Do Not Create Solid in synchronous Surface Creation

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Even when working from memory, you are spot on Alex.

There indeed is one - staring right in to eyes.

  

I see a circular opening on the surface which needs to be closed off.

 

 2016June16_02.png

 

Used a bounded surface and stitched the two without problems.

 

Then right-click on the Stitch in the PathFinder to select 'Attach' when Solid Edge asks the question.

Select 'Add'.

 

2016June16_03.png

~Tushar

Re: Stitched Surfaces Do Not Create Solid in synchronous Surface Creation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi 

 

Thanks. I could seen it because of the co-ord system. 

 

Rgds

 

Rajkumar 

Re: Stitched Surfaces Do Not Create Solid in synchronous Surface Creation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Is there any way to find the unstiched surface automatically

Re: Stitched Surfaces Do Not Create Solid in synchronous Surface Creation

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

This command is available under the Stitched command.

I purposely changed the shading to wireframe so that all open edges that are highlighted can be seen.

  

@Raj_I-value And since this is another question, I'd insist you mark it as accepted solution as well if it answers your query.

This trend has to sent in.

 

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group

 

And this video shows the steps: