Cancel
Showing results for 
Search instead for 
Did you mean: 

Stitching surfaces

Valued Contributor
Valued Contributor
I have imported a part copy with surfaces created in Solid Edge. I am trying to make some modifications and get some new surfaces stitched into it but I get a message "Stitch Failed: Unable to stitch to a single sheet". When I use the Geometry Inspector I don't find any faults. Any idea of how to sleuth the problem with this surface? Regards Peter Smith
3 REPLIES

Re: Stitching surfaces

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would assume either gaps or overhangs that are greater than the stitch tolerance.  Geometry Inspector won't find them because they aren't faults.  You may be able to use the Intersect, Trim, or Extend commands to fix this if that is the issue.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: Stitching surfaces

Gears Phenom Gears Phenom
Gears Phenom

show non-stitched surfaces will give you a quick look at the areas that still need attention.


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Stitching surfaces

Valued Contributor
Valued Contributor

I will give that a try....I can't find any obvious either overlapped or unstitched edges....but will check more closely.

Regards

Peter