Cancel
Showing results for 
Search instead for 
Did you mean: 

Strange behavior of coordinate dimension after reattaching

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Hello,

 

I updated some PEM studs on a part and had to reattach a couple of coordinate dimensions.  They are not in line with the others so I wanted to move them into place.  When I select the dimension, however, it only wants to stretch downward in an uncontrolled manner.  No matter which way I move the mouse, the dimension only goes down.  Here is a Jing video showing the issue:

 

http://screencast.com/t/H5srf9MfaS

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1
3 REPLIES 3

Re: Strange behavior of coordinate dimension after reattaching

Gears Phenom Gears Phenom
Gears Phenom

No idea if this helps, but have you broken the alignment set?

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Strange behavior of coordinate dimension after reattaching

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@kjoiner It appears to be a bug.  Others have seen this too.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com
Highlighted

Re: Strange behavior of coordinate dimension after reattaching

Pioneer
Pioneer

Similar behaviour in diametric dimensions as well, if you pick a point as the axis centre, you cannot control which axis SE dimensions. You can get around it by selecting an axis as the first point.

 

dg