Cancel
Showing results for 
Search instead for 
Did you mean: 

Strange choise of default settings

Gears Phenom Gears Phenom
Gears Phenom

Every new version I can't believe some super settings are default turned off. Can someone explain why??

Everytime I need to digg and search where these settings are located.

 

Part/sheet metal: Indicate under-constrained profiles in PathFinder (Options - General)

Part/sheet metal: Relationship Colors (Tab Inspect)

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user
1 REPLY

Re: Strange choise of default settings

Joris,

 

I agree with you in wanting some of these as default.

 

I believe the default setting are those that minimize the need for more computation and thus provide better performance.

 

Remember that there are those that are starting out with no prior experience,  so the 1st hour of using the software is critical... if there are extra icons and colors and such that the new user did not specify it my lead to confusion and in some minuscule amount it may degrade system performance.???

 

just trying to see it from a "global" perspective.  but I agree that the advanced user would like these things to remain set.

 

Ideally this is not a matter of default setting but rather a tool that stores ALL setting during upgrade, crashes, MP, or just to share with a colleague.