Cancel
Showing results for 
Search instead for 
Did you mean: 

Sub-Assemblies In Exploded Configuration

Creator
Creator

Hi,

 

I am doing manually exploded views of upper level assemblies and cannot select an entire subassembly within the upper level assembly. I have to go through and select each individual part in the subassembly to explode it. Am I missing something or is there a way around this? Thanks for your help in advance. 

4 REPLIES 4

Re: Sub-Assemblies In Exploded Configuration

Gears Phenom Gears Phenom
Gears Phenom

within the Explosion environment...  you are looking for "BIND".  this will bind sub assemblies to act as a single unit


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Sub-Assemblies In Exploded Configuration

Creator
Creator

Thank you!

Re: Sub-Assemblies In Exploded Configuration

Pioneer
Pioneer

Hello!

 

This bind option can be found only under automatic explode menu which I never use. Is there any other method to select fast patterns and assemblies?

Re: Sub-Assemblies In Exploded Configuration

Phenom
Phenom

@Reseter Bind command is not under auto explode, it is to the right of the explode icons.

 

Paint.png

 

I am not aware of a way to select the entire set of a pattern. I believe you must choose each instance individually.

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317