Cancel
Showing results for 
Search instead for 
Did you mean: 

Surface Sweep Command Does Not Allow More Than 3 Paths

Creator
Creator

Hi Community,

 

See enclosed, why can only 3 out of 4 paths be selected before moving to the cross section sub-step. The guide path keypoint curves are all identical in geometry and connected to the cross section in the same way. 

 

 

Thanks in advance Smiley Happy

2 REPLIES 2

Betreff: Surface Sweep Command Does Not Allow More Than 3 Paths

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Ji @MisterHon

 

 

sorry for that silly question, but why do You need a sweep surface for such a geometry?

 

If more path curves are necessary You also can use BlueSurf instead, or You use a Loft Feature rather than a Sweep.

 

regards
Wolfgang

Betreff: Surface Sweep Command Does Not Allow More Than 3 Paths

Gears Phenom Gears Phenom
Gears Phenom

@hawcadgood question! It's a simple extrusion (surface or body).

 

You can "only" 3 paths in Sweep command (F1 helps).

 

BR,

 

 

Imics
http://solidedgest.wordpress.com/