Cancel
Showing results for 
Search instead for 
Did you mean: 

Sweep Cut Around I.D. / Sphere (Ordered)

Valued Contributor
Valued Contributor

Having trouble cutting out a chamfer with a flat around a c'bore that goes into a round face.  Wondering if anyone can help with a better technique.  The .005 flat must remain parallel to the bottom of the c'bore, but as it sweeps around the c'bore, the whole sketch is constrained to the large radius.  I need it to constrain to the c'bore and follow the radius.  Anything other than the standard default sweep options fail.  See below and thanks in advance...

 

1.JPG

3.JPG

2.JPG

2 REPLIES 2

Re: Sweep Cut Around I.D. / Sphere (Ordered)

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Did you try the Swept Cutout - Axis button on the commandbar (next to Finish)?

Try setting axis to the center of the hole.

LMGi
www.TLMGi.com
Highlighted

Re: Sweep Cut Around I.D. / Sphere (Ordered)

Valued Contributor
Valued Contributor

That made it work.  Thanks a million Jason.

 

Matt