Cancel
Showing results for 
Search instead for 
Did you mean: 

Sweep cut?

Honored Contributor
Honored Contributor

Is the only way to do a sweep cut is to create a sweep object then Boolean subtract it? Or is there a Sweep cut command that is not set up by default in the menu's?

 

Attached is a tube where I would like to end up weth weld preps that have a 1/16" land. The cham varies because the cuts are at angles.

 

5 REPLIES

Re: Sweep cut?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

There is also the possibility to do a sweep cutout:

Type sweep in the command foinder and swept cutout will be there to

 

Re: Sweep cut?

Valued Contributor
Valued Contributor
Command finder is a good tool when you're looking for little used commands.

CAD/CAE Manager
ST8 MP12

Re: Sweep cut?

Honored Contributor
Honored Contributor

Almost everything I do is sheet metal. So a sweep cut is something I had never used.

When you look at the menues, it just states sweep.....but it's really sweep cut.

 

Thanks

Re: Sweep cut?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@12GAGE,.....difference being, there is two tool sets, one Sweep in the "Add" tools, and also in the "Cut" tools.

 

Sweep_Add.png Sweep_Cut.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Sweep cut?

Phenom
Phenom
Yeah, I really hate that. SolidWorks has the same thing..dumb..either you are adding material or removing material the function is the same. Put it all under one command and have the user select which option or like synchronous determine which is correct by the existing geometry.