Cancel
Showing results for 
Search instead for 
Did you mean: 

Swept Body Cutout

Pioneer
Pioneer

I am trying to use a "Solid Sweep" in the attached document.  I've added a body with the tool I want to act as the cutting mechanism but solid edge just keeps throwing me unknown errors without further direction.  There also doesn't seem to be alot of videos on Youtube on the subject.

 

can someone spare a second to have a look at this?

1 REPLY 1

Re: Swept Body Cutout

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JordanMcB,

 

Try expanding the "Design Bodies" collector, and right click to "Activate" back to the primary body....then the Solid Sweep tool will function as expected. 

 

Also...if you don't already know, make sure to check the "PromptBar" at the bottom of the screen [is dockable, so can be anywhere, really] for what Solid Edge is looking for next.

 

2017-01-16 (3).png

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000