Cancel
Showing results for 
Search instead for 
Did you mean: 

Switching computers, minimize setup

At work, I am getting ready to get a new workstation that is more up-to-date and more of a CAD workstation than what I have (mine is getting old and outdated).

 

Anyways, I know I can copy the "Options" file and direct to it on the new system, but is there anything else that I can copy over to minimize setup?  Most things like Holes such are already directed to a server location.

 

One think I know I would not like to lose is preset "Table" options & Holes that I have saved the settings to.  What file are these located in?

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments
5 REPLIES 5

Re: Switching computers, minimize setup

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Here's my take on the issue. I'm not sure where saved table settings are saved. Likely in a file in template\reports. Maybe in draftlist.txt.

If no one chimes in I would save a table's settings and see what file in that folder changes date/time.

 

Ribbon themes:
C:\Users\username\AppData\Roaming\Unigraphics Solutions\Solid Edge\Version 10x\Customization

Default settings: (under C:\Program Files\Solid Edge ST8...)

Custom hole settings, view scales, etc. are saved in ...\preferences\custom.xml
Custom BOM styles are saved in ...template\reports\draftlist.txt
Custom callouts are in ...\template\reports\draftcallout.txt
Custom weld symbols are in ...\template\reports\draftweld.txt
Templates are in ...\template
Materials are in ...\preferences\material.mtl.

Global settings for SE to find most of these things via the file locations in SE options reside in \preferences\options.xml.

 

Edit: appears to be in usertable.txt.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Switching computers, minimize setup

Honored Contributor
Honored Contributor

I was given the attached document from Ally PLM before upgrading from ST6 to ST7

 

In general I think:

Frame sections

Hole database

Gage table (XLS file)

Drafting templates

Annotation call outs

File templates in general (Assy, Sheet metal, part)

Re: Switching computers, minimize setup

Legend
Legend

I saved the entire solid edge folder to a network, so I didn't lose anything during the transition.

ST8 MP9
Go FAST, or go home.

Re: Switching computers, minimize setup

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@BoatTech Realise that won't include your customized menus.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Switching computers, minimize setup

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

ST9 on, this gets way easier!!!

 

http://www.engineering.com/DesignSoftware/DesignSoftwareArticles/ArticleID/10907/A-Sneak-Peek-Into-S...

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com