Cancel
Showing results for 
Search instead for 
Did you mean: 

Sychronous Technology features?

N/A

Hi,
I am trying to understand the Synchronous Technology in SE ST5.
Suppose I am in the Ordered environment. Now I create a extrude feature say EXT1.
Now I go to the Synchronous Environment & create another independent extrude feature say EXT2.
Now if I RMB on EXT1 in history tree then it shows me an option of "Move to Synchronous". After clicking that, it moves EXT1 to the Synchronous History tree.
So bringing feature from Ordered to Synchronous is possible.
But what about the other way round.
When I click on EXT2 & RMB then it does NOT show any option like "Move to Ordered".
Why is this so?
Is it not possible to bring features from Synchronous to Ordered?
Thank You.

2 REPLIES

Re: Sychronous Technology features?

Phenom
Phenom
No, it is not possible. The point of synchronous is to get rid of the history tree, and it is a one-way trip. Once moved to synchronous, this history tree is discarded and a feature cannot be moved back.
-Dylan Gondyke

Re: Sychronous Technology features?

N/A
ok, thanks chally!