Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Symbols in dimension prefix

Pioneer
Pioneer

How can I get the symbol  alpha in the dimension prefix

15 REPLIES

Re: Symbols in dimension prefix

Legend
Legend

Generate in office or google and copy/paste in prefix Man Very HappyMan Tongue

 

Edit: There is a Symbold and Values (Top left in prefix aera) option, but alpha is not in it but if you want some other standard symbols take a look at it.

Sander
The Netherlands

Betreff: Symbols in dimension prefix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KurtCouffez

 

 

 

no need to go to Office or Google, just do it in SE itself.

 

If You start to create a text box You will find the Symbol button in the Smart Ribbon Bar (right)

This will give You the abillity to find every character/sign/symbol available.

 

Copy it and paste it into the Dimension Prefix field

 

20181206_1102.png

 

 

 

regards
Wolfgang

Betreff: Symbols in dimension prefix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KurtCouffez

 

 

 

as shown in the previous post, the UNicode number for the Alpha sign would be "U+03B1"

 

I thought it should be easy to enter this code similar to an ascii code using ALT+number but this doesn't work here.

Even if You compute the decimal number of 03B1 which is 0945, but this bring a different result.

 

 

regards
Wolfgang

Betreff: Symbols in dimension prefix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KurtCouffez

 

 

just found a real astonishing behaviour in SE

 

 

Using ALT#945 creates a wonderful alpha sign in a callout text, but a strange character in a dimension prefix field

 

20181206_1132.png

 

 

The same strnage character as when typing it here in the post form:

 

now ALT+945 is shown as

 

But at least within Solid Edge I had expected it to be the same everywhere.

And Yes the font is the same for both!

 

regards
Wolfgang

Re: Symbols in dimension prefix

Pioneer
Pioneer

if I do that I will get another symbol. Even if I choose the correct font under "view - styles - dimension", I continue get other symbols. For example, under the "symbol" font, the key combination ALT97 is the letter alpha, but this does not work

Betreff: Symbols in dimension prefix

Pioneer
Pioneer

This is also the way I try, but this does not seem to work out :-(

Re: Symbols in dimension prefix

Phenom
Phenom

Alt + 224 = α

Alt + 225 = ß

Alt + 228 = Σ

Alt + 234 = Ω

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Symbols in dimension prefix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @nominus38

 

 

sounds great but doesn't work.

 

Using Alt+224 in Solid Edge creates a strange character "Ó"

 

Same is true here in the posting window

 

regards
Wolfgang

Re: Symbols in dimension prefix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad ALT+224 creates the alpha character for me both in SE and here...  α



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com