Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Re: Symbols in dimension prefix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@KurtCouffez  Here is a helpful list of ALT codes for symbols.

 

https://www.alt-codes.net/



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Symbols in dimension prefix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

thanks a lot for that info, but this IMHO means, that the result has to do with some operating system issues.

 

So when I just now type Alt+224 (Num Block) this is the outcoming result: "Ó"

And the same is created in SE.

 

I am on Win 10 prof. German with SE 2019 MP03

 

But since this happens at operating system level too, I do not think that SE ius taken any influence to that behaviour, isn't it?

 

Are You on Win 7?

regards
Wolfgang

Re: Symbols in dimension prefix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

 

 

again thanks for answering, and in the meantime (tanks google) I have found, that this is not only a personal problem, it is found often.

 

See for examplte this page:

 

https://superuser.com/questions/449029/why-does-alt224-return-%C3%93-instead-of-alpha

 

 

and many other when searching for "Why does [Alt+224] create ..."

 

Till now, none of the given hints has changed anything here.

 

Still trying to find a solution too!

 

regards
Wolfgang

Re: Symbols in dimension prefix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad  I'm using Windows 10, English language.

 

It may have something to do with the Font used as I believe each font can have different graphics representing identical address registers.  I'm using standard Arial.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Symbols in dimension prefix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

 

font I suppose is not the reason, since I have changed it to several different fonts and my personal preference also is Arial.

 

For me it looks like as this is a country/language issue if reading those several post, which were found for the "Alt+224"  search .

 

I think I have to accept this situation and this behaviour, at leas as long as anybody out there will find a better and working way.

 

 

regards
Wolfgang

Re: Symbols in dimension prefix

Phenom
Phenom

Is it possibly due to language settings or maybe different keyboard layout issues? Because mine has always been the same, although yes it does sometimes change with font. But much like Ø (alt + 0216 or a smaller one ø (alt + 0248)) degrees °(alt + 248) or my favorite, the first two letters of TOOL's 3rd album Æ (alt + 0198) they are burnt in my memory and nearly always have worked the same. For me, at least.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"