Cancel
Showing results for 
Search instead for 
Did you mean: 

Symmetric Offset Dimension Not Shown

Experimenter
Experimenter

Using Symmetric Offset command to create slot from a line.  How do I get the slot width/radius/diameter dimension to show?  (In Sychronous mode.)  Mid-point of line is on origin and it shows as fully defined even though the slot width/radius/diameter dimension is not dimensioned.

4 REPLIES

Re: Symmetric Offset Dimension Not Shown

Phenom
Phenom

Probably because there are several options for the symmetric offset (end type etc), so the dimensions are driven by the offset properties.

Why not use the slot feature - the centre axis is locatable for placing axial alignments.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.

Re: Symmetric Offset Dimension Not Shown

Experimenter
Experimenter

I just tried the Slot command (Hole pull down menu).  It has the same issue, it doesn't show the width or radius of the slot in the part or drawing mode.  "Retrieve Dimensions" did not pull the width/radius into the drawing view.

Re: Symmetric Offset Dimension Not Shown

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @filipiakt,

 

In Synchronous, the sketch geometry is used primarily to place face[s], then it is expected the user will apply the required PMI dimensions to control those "resulting faces".

 

Capture.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Symmetric Offset Dimension Not Shown

Phenom
Phenom

It is the same for a slot as for the offset command - dimensions are driven by the properties as there are several options available, dimensions are not applied.

You could say the same for holes.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.