Cancel
Showing results for 
Search instead for 
Did you mean: 

Sync Multi-body parts v ordered - Inconsistent behaviour?

Valued Contributor
Valued Contributor

Hello,

 

I am currently reviewing the Sync side of SE (ST8) with a view to driving wider use within my company.  There's lots of useful information and videos on this site which has been a great help.  As part of this process gaining a greater understanding of how ST works, its strengths and weaknesses is important in view of any internal discussions we have.

 

As part of the testing we looked at multi-body parts in the sync environment.  The part in question is not important more the process and my understanding of why it behaves as it does.  I believe I understand but would like to throw this out to the group so somebody more knowledgeable and expereinced than I can clarify for me.

 

Test MB (Sync) part in question.  

[RHinge-MB_GH2.par].jpgSync MB Part

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

[RHinge-MB_GH2.par]Failure.jpgMB Failure

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Try to move the boss either via the torus or edit the 180 dim.

 

If I did the same edit in a single body Sync part then this failure does not occur.  I believe the issue is down to the face on the web which was created tangent to the boss and therefore any move wants to change the size/shape of that face which in a MB part using sync is not possible?  I've tried the various options in the command as well as turning off all design intent.

 

I created a similar MB part in ordered and used a sketch to control size etc.  When I change the same 180 dim then the part updates as a single body sync part in that the faces tangent to the boss adapt at their angle changes due to the boss moving.

 

Bracket_Ord.par_Variable Table.jpgOrdered part

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

I hope that all makes sense.

 

Thanks,

Guy

 



CAD/CAE Manager
ST8 MP9
13 REPLIES 13

Re: Sync Multi-body parts v ordered - Inconsistent behaviour?

Phenom
Phenom

Not really a sync user, but a quick test shows you can create a concentric relationship between the axes of 2 cylinders, each in different bodies.

So in your case, this should enable you to move the boss and have the mating face of the web move at the same time.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.

Re: Sync Multi-body parts v ordered - Inconsistent behaviour?

Valued Contributor
Valued Contributor

It's the web that causes the issue, delete the web and you can move the boss.  I believe it is the face mating the web to the cylinder which is unable to chnage size/shape in the MB sync part which causes the failure.  I'd like to know if other think I am correct in saying so and if so then is this working as intended or could it be considered a 'bug'?

 

Thanks,

Guy



CAD/CAE Manager
ST8 MP9

Re: Sync Multi-body parts v ordered - Inconsistent behaviour?

Phenom
Phenom

Ok. I didn't take the test far enough.

Have to agree with you it doesn't work.

For me this is yet another example of the limitations of sync modelling.

There may be fancy ways round the problem, but that isn't the point - it should be simple.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.

Re: Sync Multi-body parts v ordered - Inconsistent behaviour?

Phenom
Phenom

Ok, I sort of have this working, by applying relationships.

Concentric for the 2 cylindrical faces.

Tangency between top face of web and the boss.

Tangency between bottom face of web and boss.

 

 

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.

Re: Sync Multi-body parts v ordered - Inconsistent behaviour?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Removed post since I overlooked the multi-body part in the question.

Re: Sync Multi-body parts v ordered - Inconsistent behaviour?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,



You also can solve that with live rules only.

But therefore You must turn on the tangent contact20160622_1415.PNG live rule too!

 

 

regards
Wolfgang

Re: Sync Multi-body parts v ordered - Inconsistent behaviour?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I could make it work using either @beachcomber's or @hawcad's solutions.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Sync Multi-body parts v ordered - Inconsistent behaviour?

Valued Contributor
Valued Contributor

Thanks guys, OK one final question. Using live rules is there a setting which means the rib will maintain the correct association with the base? In a single body part the tangent connections would adapt to allow the boss to move rather than as happens in the MB part (as I have it).

[RHinge-MB_GH2.par]_Tangent.jpg

 



CAD/CAE Manager
ST8 MP9

Re: Sync Multi-body parts v ordered - Inconsistent behaviour?

MLombard
Retired

If you applied locked dimensions, wouldn't that do what you are asking?

Retired Community Manager for Solid Edge. This account is no longer active.