Cancel
Showing results for 
Search instead for 
Did you mean: 

Synch-Sheet Metal Thickness How to change?

Valued Contributor
Valued Contributor

I'm practicing synchronous sheet metal.
I want to change the thickness after completing the modeling.
I do not think there's a way.
Can not it be synchronous?
Is it really not true?

 

youtube video : https://youtu.be/Y9JWUu5YHlw?t=427

4 REPLIES

Re: Synch-Sheet Metal Thickness How to change?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Unless I am missreading you - simply double click on Material in the Path Finder. This will open the Material Table. Now select the Guage Properties tab and make the changes you want.

 

gauge.JPG

 

Cheers

Mark

Betreff: Synch-Sheet Metal Thickness How to change?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

again I must apologize for this late answer, but at the moment an answer via tablet (andorid) or phone doesn't work.

 

The easiest way to change the material thickness IMHO is via the avriable table.

Just go into it and change the value for material thickness to the value You need.

 

Should change Your model appropriate

20170106_0913.PNG20170106_0914.PNG



regards
Wolfgang

Re: Synch-Sheet Metal Thickness How to change?

Valued Contributor
Valued Contributor

Thank you.
Today I was worried all day because of this problem.
It was a problem to include the thickness when pulling the flange.

It seems to have resolved roughly.

To use synchronous, I need to change a little bit.

Thanks to the synchronized study.

Re: Synch-Sheet Metal Thickness How to change?

Honored Contributor
Honored Contributor

I personally would not recomend Sync for sheet metal. But that's just me. I create everything from scratch and don't use other files.

 

The point I think would be important for you is the bend radius. This is the big problem with sheet metal design is estimating what the bend radius will be with your materials and tooling. As a starting point use the thickness as the radius.

 

For example I have two different 10 gage carbon steel gages in my gage table. One for short bends one for long bends. A 6 " part is bent much tighter than an 8' part being bent on the same machine.

 

The bend radius controls many things. Most importantly the size of the flat pattern around the corners. 

 

Set K=0.33 and call that part of it done. Many consider K=0.29 a better approximation for hems, but I find that distinction not worth the effort for low tolerance steel fab.