Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: Synchronous Body Relationship Assistant?

Gears Phenom Gears Phenom
Gears Phenom

@bshand

 

Bruce,  hahaha...  hopefully someonce can create a short video..  i will try to sneak in some time but cant promise...

 

HTH = Hope that Helps...   but obviously it did not...

 

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: Synchronous Body Relationship Assistant?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Johnson_BigMatt, A video would be greatly appreciated. Sometimes I need a 2x4 to the head.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Betreff: Synchronous Body Relationship Assistant?

Gears Phenom Gears Phenom
Gears Phenom

@bshand

babbeled on a bit but see if this helps...   with audio.../

(view in My Videos)

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: Synchronous Body Relationship Assistant?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Thanks @Johnson_BigMatt, that's an effective 2x4. My experimental model was too simple, a cube, I think for it to reveal much.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Betreff: Synchronous Body Relationship Assistant?

Valued Contributor
Valued Contributor

hi~ Matt

Thanks for the videos and answers.
There are settings in the video that save the design intent.
This is valid until the solid edge is completely terminated.
But when you re-run Edge and open it, it's back to its original state.
We are a structure that returns people who are needed for a network license.
Sometimes you have to turn it off completely and run it again ...
In my view, it is like storing.