Cancel
Showing results for 
Search instead for 
Did you mean: 

Synchronous Dimension

I can't figure out how to create the dimension shown below in Synchronous. Every time I try to create the dimension, it wants to snap to the center of the radius but I want to dimension the flat. I have attached the part file. Any ideas? 

 

sync_dim.png

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10
5 REPLIES

Re: Synchronous Dimension

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

That is strange and don't know the reason why.

I placed the dimension and then using Alt+Drag attached it to the desired end point.

 

2016022601.png

 

~Tushar

 

Re: Synchronous Dimension

Phenom
Phenom

Hi,

 

Could you please show your dimension bar, if you are using all the snap points?

 

Yasser

 

dimension_all_snap_points.jpg

Re: Synchronous Dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I agree with Tushar. It's weird that it snaps to the center of the arc rather than the selected endpoint.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Synchronous Dimension

Phenom
Phenom

When I try this it attaches to the endpoint, but then is unmodifyable.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Synchronous Dimension

Thanks for the replies. I have submited to GTAC.

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10