Cancel
Showing results for 
Search instead for 
Did you mean: 

Synchronous Feature Mirror?

Valued Contributor
Valued Contributor

I use a mirror function in a synchronous.
The feature is a mirror surface.

How can the mirror is a solid?

Sunch Mirror.png

The attached file.

 

6 REPLIES 6

Re: Synchronous Feature Mirror?

Phenom
Phenom
Try to select the inner and outerfaces too ! Then it should work

Yasser

Re: Synchronous Feature Mirror?

Phenom
Phenom

It doesn't work because the side face of the feature is planar to the side face of the box.

Syncronous can't appear determine the boundary where the feature and box join.

It is the same if you try to create a circular pattern of a similar feature around a cylinder - if the end of the feature is planar to the end of the cylinder it doesn't work. One of the limitations of sync.

Just to clarify - I am using ST7, so things may have improved in later versions.

 

EDIT: Sorry, the cylinder example I gave now appears to work - didn't used to though

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Synchronous Feature Mirror?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I'd recommend using the Selection Manager to recognize a Rib/Boss from the face and then mirror it as below:

 

 

~Tushar

Re: Synchronous Feature Mirror?

Phenom
Phenom

It's working apparently Smiley Happy

 

Synchronous Feature Mirror

Re: Synchronous Feature Mirror?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @beachcomber

 

Same technique of using the Selection Manager as in the previous video of this thread works for me with patterns as well:

 

 

~Tushar 

Re: Synchronous Feature Mirror?

Valued Contributor
Valued Contributor

Thank you good answers.
And who made you and Find Where used Part to Draft Direct Application well used.
Love it...^^