Cancel
Showing results for 
Search instead for 
Did you mean: 

Synchronous holes

Creator
Creator

In synchronous, is there a way to combine identical hole instances from different hole features into the same feature?  I know I can open the hole options in an existing feature by double clicking the hole and select "more holes" to add additionals, but can I take existing holes in a different feature and combine all hole instances into one feature?

 

On a similar token, can I combine separate Face Relationships into one?  Let's say I have two holes and I give them a coplanar axis relationship.  Then I add another hole.  I want the new hole to be in line with the other holes.  I know I can add a new coplanar axis relationship, but can I edit the first relationship to include the third hole?  Or do I just have to delete the relationship between the two holes and add a new one to include three holes?

 

Thanks

4 REPLIES

Re: Synchronous holes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

there is one way, which I use therefore.

 

First convert the holes (both features) to surfaces, that means simple features.

And then run the hole wizzard.

It will recognizes this "free" holes an will build a new combined hole feature.

 

It would be fine, if this would be integrated into standard SE procedures.

 

Thee is also another ER I think:

A method or special shortcut, when copying holes with the wheel, to put the copies into the existing hole feature group.

 

regards

Wolfgang

 



regards
Wolfgang

Re: Synchronous holes

Creator
Creator

Do you know of a quick and easy way to convert Hole features to simple features?

 

Thanks,

 

Eric

Re: Synchronous holes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @ericderace

 

 

 

Yes, simply push the RMB when selecting the holes and go to "Break Hole" 

 

 

20170315_1648.PNG



regards
Wolfgang

Re: Synchronous holes

Creator
Creator

Awesome, thanks!