Cancel
Showing results for 
Search instead for 
Did you mean: 

Syncronous / Ordered

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Hello Everyone,

What is the advantages to use ordered in place of syncronous? *When is better to use ordered?

Thx!

3 REPLIES 3
Highlighted

Re: Syncronous / Ordered

Creator
Creator

Actually both are good at what they can do and in a mixed "Hybrid Modeling" envirnment SE does really well, look at

 

https://community.plm.automation.siemens.com/siemensplm/attachments/siemensplm/solid-edge-tkb/371/1/...

Re: Syncronous / Ordered

Honored Contributor
Honored Contributor

Sync is good for imported parts from other system and Non-sheet metal parts.

 

I don't use sync because my focus is sheet metal.

 

The area Sync really falls down is flat pattern controls and editing the gage of a material (Gage = Thickness and Bend radius)

 

Also w/ frames you have to make a choice early on. The Frame sections have to be either sync or ordered. I chose ordered.

 

Within a single part, you can do ordered work on top of Sync, but you can't do Sync work on top of Ordered. If this was the other way around I would be VERY motivated to use Sync. 

 

I need the "basics" of my models to be ordered. Since I can't use sync on top of ordered, I don't use it at all.

 

From a conceptual standpoint, ordered maintains relations to creation sketches. In sync, sketches are used to start part creation, but once the part exist, the sketch removed.

Re: Syncronous / Ordered

Phenom
Phenom

Hi,

 

If you need to have 100% control of your sketch you should use Ordered.

With complicated Geometries you have to edit the Sketch more than on time and this is guarantied with Ordered.

 

But I like and use Synchronous "with Sheet Metals too". Just in view cases for examples "Rail profiles" I used Ordered to be able to control every details and make controled changes.

 

Yasser