Cancel
Showing results for 
Search instead for 
Did you mean: 

Table of line lengths by layer

Experimenter
Experimenter

Hi there, I need to be able to create a table of line lengths, ideally grouped by layer...

is this possible? 

1 REPLY 1

Re: Table of line lengths by layer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Nothing automated that can do this.  You can make each line a block and then use a Block Table to list them, but you would have to enter block attributes for length and layer to be able to have that info in the table and be able to sort it.

 

Otherwise, if you have access to the API (Free2D does not) you could write a program in VB to do this.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com