Cancel
Showing results for 
Search instead for 
Did you mean: 

Tangent Dimension

How can I create a tangent dimension in the position shown? The tangent dimension keeps snapping to either a vertical or horizontal position.

 

tangent_diameter_dimension.png

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10
4 REPLIES

Re: Tangent Dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @David_McMahon,

 

Don't think ther is a function to place that type of dimension automatically......however, a workaround would be to place a fine line sketch, using draw-in-view, and then return to the working sheet to place a smart dimension on that line.

 

Draft1.jpg

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Tangent Dimension

Phenom
Phenom

You can do that - on the dimensioning toolbar there is a tangent option

Click that before selecting the first circle/arc and you can dimension tangent to tangent.

Dim tangent Option.JPG

 

 

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.

Re: Tangent Dimension

Gears Phenom Gears Phenom
Gears Phenom

Look at the position from his dimension. Man Wink

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Tangent Dimension

Phenom
Phenom

@Joris - Ok, I'll give you that one. Smiley Wink

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.